About Us
The name Elster has been associated with high-quality and innovative gas measuring and regulating devices for more than 170 years. Today Elster manufactures energy measuring systems, ultrasonic, turbine, rotary and diaphragm meters as well as gas pressure regulators for low, medium and high pressure. Electronic station flow computers, volume correctors, innovative data read-out and evaluation systems as well as automatic remote data read-out devices are in the electronics products range. Furthermore turnkey gas regulating and measuring stations of every size or test rigs for calibration of custody transfer gas meters complete the range of products focused on gas.
Facts and milestones in product development
- 1836
Formation of the American Meter Company - 1848
On the 1st of October, Elster was founded in Berlin and began producing gas lamps. - 1853
Production of large station gas meters. - 1865
Formation of G. Kromschroeder AG. - 1876
The factory in Mainz was built. - 1878
Emil Haas obtained a patent for the principle of a rigid limited space for the volume measured, which is still valid for the production of our diaphragm gas meter today. - 1936
The first horizontal turbine gas meter was launched. - 1952
PTB approval was granted for the first horizontal operating turbine gas meter (PTB = German Approval Authority). - 1955
Development of the first mechanically driven volume corrector. - 1961
Development of the Quantometer for in-plant measurement. - 1965
Foundation of Instromet in the Netherlands. - 1971
SM-RI Turbine Meter and Q-RI Quantometer were launched. - 1976
Development of a turbine gas meter with interchangeable measuring cartridge suitable for calibration. - 1980
Development and production of electronic volume correctors and flow computers by Instromet. - 1981
Establishment of an instrument flow computer and volume correctors division in the UK - 1982
Development of SM-RI Turbine Meter and Q-75 Quantometer Multi-Index.
Approval was granted for the first electronic volume corrector called EMU that uses micro process technology. - 1987
Announcement of the long-term pulse collecting system called LIS-100 to the global market.
Launch of the BK-G4 Diaphragm Gas Meter with improved performance. - 1990
Launch of a battery-driven EK-88 Volume Corrector and the GAS-ASS station management system by FlowComp. - 1991
Launch of an IRM-A Rotary Meter. - 1992
Process gas chromatographs developed for energy measurement. - 1993
Introduction of mechanical temperature correction on BK-G4 and BK-G6. - 1995
Launch of a RVG Rotary Meter series.
Development of the ultrasonic meter for non-fiscal metering. - 1997
Development of the M2R Compact Gas Pressure Regulator (max 4 bar). - 1999
Launch of the IRM-3 Rotary Meter. - 2001
Development of a new generation of volume correctors known as EK210 and EK230 and of gas meters with an Absolute-ENCODER technology. - 2003
Flow Comp gas-net product line launched. New generation of industrial diaphragm gas meters BK-G40 and BK-G65.
PTB approval for a gas analyser system gas-lab Q1. Launch of high-pressure regulator MR 50. - 2004
Introduction of the modular index concept Z6 for diaphragm gas meters, together with CHEKKER and Absolute Encoder technology. - 2005
Merger of Elster and Instromet. Turbine meter series TRZ2 were launched. - 2006
Introduction of the new industrial diaphragm gas meter BK-G100. Approval of the air operated closed loop high pressure test rig in Mainz. - 2007
PTB approval for Encal 3000 gas chromatograph.
- 1891
11. April 1891: Gründung der Firma "S. Elster OHG" in Wien 5 mit den Gesellschaftern Johannes Ferdinand Siegmar ELSTER und Conrad Otto Ferdinand ELSTER.
Gegenstand des Unternehmens:
Fabriksmässige Erzeugung und Reparatur von Gasmessern, Gaskoch-, Heiz- und Beleuchtungsapparaten und Einrichtung von Gaswerken mit Anschluß der dem konzessionierten Gewerben vorbehaltenen Berechtigungen sowie fabriksmäßige Erzeugung von Elektromotoren und elektrischen Apparaten. - 1950
Ing. Franz Richter wird Geschäftsinhaber. - 1957
Die Firma "S. Elster OHG" wird in eine GmbH umgewandelt. Gesellschafter Johannes Siegmar ELSTER und Ing. Franz Richter. - 1962
Johannes Siegmar ELSTER scheidet als Gesellschafter aus.
"ELSTER & CO AG" in Mainz wird Hauptgesellschafter. Ing. Eduard Forster wird zum Geschäftsführer ernannt. - 1979
Übersiedlung von Wien 15, Felberstraße nach Wien 19, Heiligenstädterstraße 45. Ing. Gerhard Velek wird zum Geschäftsführer ernannt. - 1987
Nach der Pensionierung von Ing. Gerhard Velek wird Ing. Josef Franz neuer Geschäftsführer. - 1988
Ausscheiden der Fam. Richter aus der Firma. - 1989
Laut Beiratsbeschluß wird das Vertragsgebiet Österreich um folgende Länder erweitert: Ungarn, Rumänien und Jugoslawien. Gleichzeitig wird die Zweigniederlassung Gastechnic Wien des Stammhauses Straubenhardt in die Firma "S. Elster GmbH" integriert. Von Wien aus werden Handelsvertretungen aufgebaut. - 1990
Umwandlung von "S. Elster GmbH." in "ELSTER Gastechnic Produktions- und Vertriebs- Gesellschaft m.b.H."
Gegenstand des Unternehmens:
1a) die fabriksmäßige Erzeugung, Reparatur und Handel (von gas- und elektrisch betriebenen Koch- und Heizgeräten,) von Messgeräten für Gas, (Elektrizität und Wasser, von Elektromotoren,) von Apparaten, Maschinen und Geräten für die Einrichtung von Gaswerken. ***
1b) die technische Beratung, Projektierung und Entwicklung von gastechnischen Anlagen.
1c) Vertrieb von Produkten der Unternehmensgruppe der "ELSTER AG" in Mainz.
2) Die Gesellschaft ist berechtigt, sich auf ähnlichen und zusammengängenden Gebiet zu betätigen und sich an anderen gleichartigen Unternehmen zu beteiligen. Die Gesellschaft ist jedoch nicht berechtigt, Bankgeschäfte zu tätigen.
*** Die in Klammer gesetzten Textteile sind nicht mehr relevant. - 1995
Durch die Teilung von Jugoslawien in Serbien-Montenegro, Kroatien, Slowenien, Mazedonien und Bosnien-Herzegowina, wird die Vertretung von Rumänien abgegeben. - 1996
Das Kromschröder-Sicherheitsprogramm wird für Österreich (bis zum Jahr 2002 auch für Ungarn) in den Vertrieb mitaufgenommen. - 2002
Das Kromschröder-Sicherheitsprogramm wird auf Direktlieferung durch Hauptwerk Osnabrück umgestellt. Die Aquirierung erfolgt weiterhin in Wien. - 2004
Ungarn und Slowenien werden Mitglieder der EU.
Beide Staaten werden weiterhin von Wien betreut. - 2005
Nach Kauf der Instromet-Gruppe durch die Elster AG kommt es weltweit zu Zusammenschlüssen beider Firmen zur Firmengruppe "Elster-Instromet".
01. Juni: Umwandlung von "ELSTER Gastechnic Produktions- und Vertriebs- Gesellschaft m.b.H." in "Elster-Instromet Vertriebsges.m.b.H.".
1. Oktober: Instromet B.V. GmbH in Wien wird eingegliedert. Gemeinsamer Firmenname ist "Elster-Instromet Vertriebsges.m.b.H.". Standort ist 1190 Wien, Heiligenstädterstraße 45. - 2007
01. Jänner: Nach der Pensionierung von Ing. Josef Franz wird Ing. Thomas Linzer neuer Geschäftsführer.
- Elster Liège a vu le jour en 1919 sous le nom de Cogégaz (Constructions Générales Electriques et Gazières).
Pendant près de 75 ans la société acquière un savoir faire et une réputation dans le domaine du comptage et de la régulation du gaz naturel. En 1995 elle intègre le groupe Elster.
Depuis le 15 juillet 2009, Cogégaz a fusionne avec les 2 autres sociétés du groupe Elster en Belgique et devient Elster NV/SA.
Aujourd’hui le site de Liège se concentre sur 3 activités :
- La commercialisation des compteurs et régulateurs résidentiels sur toutes la Belgique
- Le comptage et la régulation industrielle en Wallonie et Bruxelles
- La commercialisation du matériel et la conception de systèmes pour les fours industriels sur toute la Belgique
- Elster Cogégaz c’est une équipe de 50 personnes au service de ses clients depuis plus de 90 ans.
- 1982
Firmaet starter i lejede lokaler i Hjørring, som filial af det USA-baserede firma Singer Symaskiner´s kontor i København.
Singer Symaskiner bestod af mange divisioner, hvoraf en var American Meter som i mere end 150 år havde beskæftiget sig med gasmålere og - regulatorer. Med basis i American Meters produktsortiment var grundstenen lagt til firmaets mangeårige leveringer til det Danske Naturgasprojekt. - 1985
Efter 3 år havde firmaet vokset sig så stor at det nu kunne stå på egne ben. Med det amerikanske selskab American Meter som aktionær blev International Gas Apparatur A/S med binavn IGA A/S stiftet. - 1987
IGA flyttede til nybygget industriejendom på nuværende Adresse. - 1988
I USA sker der en opsplitning af selskaberne i Singer-koncernen. American Meter bliver købt af det tyske selskab Ruhrgas AG, der primært beskæftiger sig med køb, salg og transport af Naturgas. - 1992
Der sker en stor omorganisering hos Ruhrgas AG. Der stiftes et nyt selskab, Ruhrgas Industrie GmbH, som skal drive koncernens industriselskaber. Et af disse, Elster AG, som siden 1848 har beskæftiget sig med gasmålere og -regulatorer køber IGA ud af American Meter. - 1993
Et andet selskab i koncernen, G. Kromschröder AG, stiftede få år tidligere et salgsselskab i Danmark, Gastechnic Danmark A/S. Det blev nu bestemt at forene de to lokale firmaer, så fra 01. januar 1993 blev alle aktiviteter i Gastechnic flyttet til IGA A/S. - 1995
IGA A/S er nu ansvarlig for hele Gruppens produktprogram i hele Skandinavien. Ud over egne produkter er det primært varer fra American Meter, Elster og Kromschröder. - 2005
Vort tyske moderselskab fusionerer med Instromet fra Belgien, og ændrer navn til Elster-Instromet GmbH. I samme anledning ændres også vort firmanavn fra IGA A/S til Elster-Instromet A/S. Vi får samtidig det fulde markedsføringsmæssige ansvar for Instromet´s produkter i Skandinavien.
The gas industry has developed in the first part of the 19-th century. Initially gas town started to be used for streets lighting. The first gas work in Bratislava was established in 1856.
In connection with the expansion of gas application it was necessary to start to measure the gas consumption by means of gas meters. The first gas meter was invented by the Englishman Samuel Clengg in 1815. It was a wet displacement meter. In 1820 John Maclam has patented the first dry gas meter and in 1843 Wiliam Richards designed a dry gasmeter with two chambers and valves. Gas meters on this principle have been using up to these days.
Gas meters production in the territory of Slovakia has started in 1922. The first gas meter was produced in the factory of the brothers Michera in Bratislava. After the World War Two the gas meter production was relocated to Považské strojárne (machine plant) and since 1952 it has been placing in Presná mechanika, n.p. Stará Turá. In 1965 the national enterprise Presná mechanika was incorporated in the industrial concern Chirana Stará Turá.
In 1992, in the process of privatization of the joint-stock company Chirana-Prema, a.s., the gas meters production was divided into an independent company named Premagas s.r.o. In 1993 the company Elster AG Mess- und Regeltechnik with its registered office in Mainz, Germany has become the majority owner of the company Premagas s.r.o. Since 2002, Elster is the sole owner of the company. Company name Premagas s.r.o. was changed to Elster s.r.o. in 2007.
Production of water meters has started in 2005 and production of regulators in 2006.
Elster s.r.o. is now part of Honeywell.
Elster Group este lider mondial in AMI (Advanced Metering Infrastructure), masuratori integrate si solutii de utilizare in industra gazului, electricitatii si apei. Inalta calitate a produselor, serviciilor, si solutiilor marca Elster reflecta bogatia de cunostinte si experienta acumulata de peste 170 de ani dedicate masuratorilor de precizie a consumurilor de resurse. Elster ofera solutii si tehnologii avansate pentru companiile de aprovizionare cu energie. Avantajele pentru furnizorii de energie: imbunatatirea serviciului de relatii cu clientii, cresterea eficientei operationale si de a creste beneficiile clientului. Cu solutiile AMI de la Elster, permit furnizorilor de energie vitala a resurselor de gaze, energie electrica si apa sa administreze si sa mentina un nivelul bun de cost-eficient. Grupul are peste 7.000 angajati in peste 38 de tari cu precadere in Europa, America si Asia.