Industry Article
Compressors Q&A with CCC
Turbomachinery controls are critical to the overall efficiency of LNG operations. In the July 2023 issue of LNG Industry, CCC’s Serge Staroselsky shared key insights into the LNG landscape from the turbomachinery controls perspective. Read the full article to explore:
- How compressors improve the efficiency of the LNG process
- Which factors to consider when deciding which compressor technology is needed for an application
- How compressors are helping to reduce emissions (e.g. carbon dioxide) in the LNG process
- How compressor technology is adapting to new and expanding LNG markets
Read “Compressors Q&A” now to gain insights into the critical role of controls in LNG compressor optimization — including how autonomous operation will continue to shape the LNG market.